Part Number: TPS65987D
Hi Team,
Could you check Type-C PD schematic designed by my customer quickly.
Please find the schematic here.
Regards,
Takashi Onawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Takashi,
1. Is PPHV considered as a source or a sink? If it is a sink, 47 uF of capacitance is recommended on that node.
2. It is recommended to have 1 uF of capacitance on the VBUS pins.
3. Please check the ADCIN1 configuration, the resistor places the divider at 0.91 * V_3p3 which would place the configuration as Configuration 5 with BP_NoWait.
4. Please check the ADCIN2 configuration, the resistor places the divider at 0.91 * V_3p3 which would place the "I2C UNIQUE ADDRESS [3:1]" as "011b."
Thanks,
Mike Emanuel
Please click "Resolved" if this solved your issue.
Hi Emanuel-san,
Thanks for your quick review.
I will tell them that to them.
Regards,
Takashi Onawa