Part Number: DP83TC811S-Q1
hello,Please provide the driver code for linux4.14, thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811S-Q1
hello,Please provide the driver code for linux4.14, thank you.
Hi there,
The drivers are available in our software tool and should work for linux 4.14
Thanks,
Cecilia
hello
The driver I found at the following url is about linux5.11.Could you please tell me the specific download address about linux4.14.
hello
Now,Ping packet error.I- read the PHY 0x01 register, which is 0x65.
Please advise me what to do next.Thank you very much!
From 192.168.30.1: icmp_seq=288 Destination Host Unreachable
From 192.168.30.1: icmp_seq=289 Destination Host Unreachable
From 192.168.30.1: icmp_seq=290 Destination Host Unreachable
From 192.168.30.1: icmp_seq=291 Destination Host Unreachable
From 192.168.30.1: icmp_seq=292 Destination Host Unreachable
From 192.168.30.1: icmp_seq=293 Destination Host Unreachable
From 192.168.30.1: icmp_seq=294 Destination Host Unreachable
0x1 = 0x65 shows that there is a link between the two devices. What type of packet errors are you reading? can you please share the rest of the registers?