This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988EVM: Factory image of TPS65988EVM?

Part Number: TPS65988EVM

Hello.

Can you share the factory image (binary data) of TPS65988EVM?

Or is there a preset in the Application Customization Tool that is the same as the factory image?

Thank you.

  • The device factory settings can be recovered via the following process:

    1. Open the Application Customization Tool
    2. Click Project -> New Project
      1. TPS65988DH
      2. Standard (Recommended)
      3. Upstream Facing Port (UFP) Only
    3.  Click Device -> Re-Flash EVM Firmware (Recovery)
      1. Select the tps65988_evm_flash_image.bin for the EVM Recovery File
    4. Click OK

    This will restore the original EVM firmware.