Part Number: PCA9548A
Other Parts Discussed in Thread: TCA9548A
Hi team,
We want to check whether the PCA9548A can support the two structures below. structure 1, remove the TXS0108 circuit and just connect the PCA9548A to 1.8v side with 4.7k pull up resistors, but the high voltage will be 2.12v and rising waveform has the return curve. Whether the device can be used for 1.8V condition and whether it has risks? Why the waveform is like this?
Whether we can use the above structure with TXS0108 for the requirement as the structure 2, if we connect like this, the TXS0108 left side also has the return curve. What's your opinion? Thanks.