This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125DF410EVM: Sigcon EVM GUI Problem : There are no USB2ANY interfaces detected

Part Number: DS125DF410EVM
Other Parts Discussed in Thread: USB2ANY, DS125DF410, ALP

1. I installed Sigcon Architect to run the DS125DF410EVM. (Windows 10 & Windows 7)

2. Both 3.3V and 2.5V are OK (LED is on)

3. Operating in Slave mode (LED is on.)

4. PC and EVM are connected through USB Cable.

5.  As shown in the figure below, the message "There are no USB2ANY interfaces detected" appears and EVM does not work.

6. Device Manager says that the NSC USB Nano driver is not installed.

What else do I need to do to get the Sigcon GUI (EVM) working?