Part Number: DP83848-EP
Hello Sir,
One of my customers is designing a board with using DP83848NRTAR. The customer wants to check:
1. if the PIN19 (PFBOUT) only connects to PIN30 (PFBIN2) and doesn't connect to PIN16 PFBIN1. Is it OK?
2. In datasheet, PIN 8, 9, 10 is floating and the customer pulls up them to 3.3V. Is it Ok?
May I send the customer's schematic to you for checking?
Best regards,
wenting