This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TPS65987D: TPS65987D e-mark can not be identify

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, TIDA-050012, TPS65981

Tool/software: TI C/C++ Compiler

Hi , 

I have same issue in TPS65987 , 

When I set 20V 3A profile to 20V 5A. by Source Board(TIDA-050012) with pjt(TIDA-050012 Source Board) 

Then using Sink Board(TIDA-050014) to Check Source Profile with "Received  Source Capabilities(0X30)",

But the Receive Source Profile still show 20V/3A , Can help me please?

(-----------My Device--------------)

Source Board:  TIDA-050012

Sink Board: TIDA-050014

Type C Cable: E-Books

TPS65981_2_6_7_8 Application Customization GUI Version : 6.1.1 

Source Board Pjt File: 

4744.SourcePjt.pjt



(1) When I connect  other type-c charger witch can provide more than  3A  to Sink board, then Check the register "Received  Source Capabilities(0X30)", it's  profile is correct  as Type-C Charger .

(2) Is there any register in TPS65987 that  can check E-mark is on or not?