Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, TIDA-050012, TIDA-050014, TPS65981
Hi ,
I have same issue in TPS65987 ,
When I set 20V 3A profile to 20V 5A. by Source Board(TIDA-050012) with pjt(TIDA-050012 Source Board)
Then using Sink Board(TIDA-050014) to Check Source Profile with "Received Source Capabilities(0X30)",
But the Receive Source Profile still show 20V/3A , Can help me please?
(-----------My Device--------------)
Source Board: TIDA-050012
Sink Board: TIDA-050014
Type C Cable: E-Books
TPS65981_2_6_7_8 Application Customization GUI Version : 6.1.1
Source Board Pjt File:
(1) When I connect other type-c charger witch can provide more than 3A to Sink board, then Check the register "Received Source Capabilities(0X30)", it's profile is correct as Type-C Charger .
(2) Is there any register in TPS65987 that can check E-mark is on or not?