Part Number: ISO1452
Other Parts Discussed in Thread: ISO1412
Hi TI,
We are facing an issue while using ISO1452 (RS485 and RS422 transceiver) in our custom board. we have a device which works on RS485. here is the command
FF 08 XX XX XX XX 0B (Modified)
and below is the response which slave should return.
FF 1C 00 02 XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX XX 06 80 80 63 6C (Modified)
but instead of only response it returns CMD+RESPONSE. (command which is sent, followed by response). I am not able to understand why it is returning CMD with response. why not only response.
here is the images
and here is the circuitry which we are using
kindly help out.
Br,
Sarju Bhatnagar