Part Number: TPD1E01B04
Other Parts Discussed in Thread: TPD1E6B06, ESD401
We are currently using PESD5V0H1BSF
Can you please suggest part similar to TPD1E01B04DPLR with 5V Working Voltage in 0201 package dimensions
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD1E01B04
Other Parts Discussed in Thread: TPD1E6B06, ESD401
We are currently using PESD5V0H1BSF
Can you please suggest part similar to TPD1E01B04DPLR with 5V Working Voltage in 0201 package dimensions
Hello Saurabh.
For a P2P bidirectional single channel part with 5 V Vrwm in a 0201 package, the only suitable device I found was TPD1E6B06. Unfortunately, this part has a much higher capacitance at 6 pF.
However, if it's possible to switch to a 0402 package, I would suggest ESD401. This is a bidirectional single channel part with 5 V Vrwm with a 0.77 pF capacitance. It also has an extremely low leakage current at 0.03 nA.
Let me know if either of these parts work for you.
Regards,
Matt Smith