This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: SN65DSI86ZQER i2c communication not working

Part Number: SN65DSI86


Hello Support,

I have designed one bridge circuit using SN65DSI86ZQER IC and i have developed circuit with help of reference circuit in datasheet and some of portion from EVM board for the same.

here all power supplies are working fine 3.3V,1.8V,1.2V but when i'm trying to detect i2c address using other host micro-controller(arduino) to verify it's working or not

but here it's not detecting any address for SN65DSI86ZQER but same host able to detect other device it means here problem is with SN65DSI86ZQER board
it should detect 0x2C as pin per configuration.

and i also want to know how to configure SN65DSI86ZQER using otherhost mcu like. arduino

i have attached schematic please check and let me know if any mistake i did and correction needed for the same.

My original application is to interface edp 10.1 inch display with Khadas VIM3 Board

and i'm using SN65DSI86ZQER as bridge ic.

Thanks .MIPITOEDP.pdf