This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E: EVM doesn't work

Genius 17975 points

Part Number: DP83TD510E
Other Parts Discussed in Thread: , USB-2-MDIO

Hello,

 

Our customer is evaluating DP83TD510E-EVM and facing a problem.
Now 2 DP83TD510E-EVMs and a network test equipment are connected like the below figure and they tested the communication between each EVM.
Then the link itself seemed to be established, but when the network test equipment sends a test flame to each EVMs, any communication between EVMs was not done.

 

The below is their jumper configuration of this EVM

 

J12(external power) : 5V

J9 (USB-5V) : Open

J14/J15/J16 : internal power

J17/J18 : 1

J19: LED_0

J20: 0 (DP83TD510E: Master, DP83822: Slave)

J26/J27 : EXT

 

They didn’t configure any registers through USB-2-MDIO.

 

What do you think the root cause is?

 

Regards,

Oba