Part Number: DP83867E
According to another e2e thread, this pin has 9KOhm internal pull up Register to PU.
When my customer use /INT mode, Customer mention /INT is default is high eventhough no-pullup-registance.
When customer implemented external 4.7Kohm, INT signal could not go to enough low level around 1.8 - 1.3V range.
Datasheet recommended 2.2Ko, So I already recommended 2.2Ko pull up instead of 4.7Ko.
Orinigally I understand following. But please correct right behavior ?
/INT : Output : OD
/PWD: Input: internal 9Kohm pull up.