This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: GPIO communication on Port1 single link situation

Part Number: DS90UB949-Q1

Hi team,

My customer want to communicate on GPIO0 from UB928 which is connected to Port1 of UB949(backchannel GPIO) but not going well.

I also check it on my EVM and, I was able to communicate both direction if I connect UB928 to Port0 but I wasn't able to communicate both direction if I connect to Port1.

I only set GPIO0 config register of both Ser and Des. What additional setting is required when I use GPIO on Port1?

UB949: 0x0D[7:0]=0x1F

UB928: 0x1D[7:0]=0x23

Please advice.