Part Number: TFP401A
Other Parts Discussed in Thread: TFP401, TFP410
I’m confusing a resolution of TFP401.
In the datasheet, I saw two sentences that confused me.
- Supports Pixel Rates up to 165 MHz (Including 1080 p and WUXGA at 60 Hz)
- The DVI interface supports flat-panel display resolutions up to UXGA at 165 MHz in 24-bit true color pixel format.
Can TFP401 support the Full HD resolution (1920x1080) when converting from DVI to RGB and from RGB to DVI?
What is the max resolution when TFP401 converts from DVI to RGB?
What is the max resolution when TFP401 converts from RGB to DVI?