Part Number: TUSB8042A
Other Parts Discussed in Thread: TUSB9261
Hi There,
I'm trying to do a compliance test under Linux Yocto OS(Kernel 5.4.45), how can I send the pattern under Linux os?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
there is the link talking about how to command the hub to enter downstream port TX compliance.

Hi Brian,
Thanks for ur reply, I have another question about USB compliance test, I have two USB 3.1 HUB(TUSB8042A), and the secondary hub upstream port connect to the first HUB downstream port 3, all the USB HUB#1 downstream port connect to IC (like TUSB9261 . TUSB8042A . etc), and all the secondary HUB connect to the USB Type-A connector, so I have to set both TUSB8042A HUB to compliance mode when I do the compliance mode test right?(USB 3.1 gen 1 & USB 2.0/1.1/1.0 test)