Part Number: TUSB9261
Hello,
I designed a pcb that is essentially equivalent to the reference design. I am having an issue with the EEPROM.
I can load the default firmware into the device without an issue and all works as expected until I unplug the device and plug it back in. Once I do this, it comes up as if it is the first time it is being powered and I see the bootloader again.
If the code isn’t being stored to EEPROM by would the device function as defined above? I am trying to determine if the firmware is getting written and then erased or never written at all.
Any suggestions?
Thanks
Jason