This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS280DF810: questions

Part Number: DS280DF810

Hi team,

DS280DF810 is used for customer 100G test project. There are two important requirements, please confirm whether they can be realized:

1. 4 ~ 8 channels, the rate is 1 ~ 28.4Gbps, continuously adjustable output (that is, any rate can be adjusted out), the receiver can also lock this arbitrary rate and error detection (error test).

2. There is a high-speed output clock. The minimum frequency of the clock is 8 division of the rate (for example, 25.78G, then the clock frequency is 3.22GHZ). It is used for oscilloscopes as trigger signals.