Part Number: DP83TC811S-Q1
A few days ago, we used EC20 and PHY dp83tc811s to communicate with each other through SGMII interface, but there was a problem that Ethernet Ping could not work.
According to the investigation, the high packet loss rate is caused by the wiring harness and the real vehicle environment. After the packet loss rate is high, the Ping will not work after 30 minutes to - 1 hour.
Conclusion
Because the signal quality on the line is not good, it will cause some error packets,
When there is a continuous error packet (from the captured SNR, we can see that there is a continuous state of very poor signal-to-noise ratio), then 4G module (using Ti dp83tc811s) sends a pause packet to 5g, and then Ping will not work
Now I want to know,
1. Is there any mechanism in the bottom layer, when the packet loss is high (the packet loss of the faulty line reaches 5% - 20%), it will directly lead to the Ping failure?
2. Why does the pause packet occur when the signal quality is poor? Is this the mechanism of this chip?