Part Number: DS90UB941AS-Q1
Hi team,
This is brandon. i have some questions on 941, listed below:
1.Both 948 and 941 have I2C, SPI, I2S, and gpio function pins. Can these functions be communicated at the same time? And it's all transparent, right?
2.For 948, can I use pin11-14 as I2S and pin9-10 as gpio at the same time? 941 can also be used in this way, right?
3.Is there a one-to-one correspondence between 941 and 948 gpio? For example, gpio2 (pin10) of 948 corresponds to gpio2 (pin38) of 941;
4.What is the difference between gpio_reg and gpio?
BR
Brandon