This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCI2050B: About PCI2050B 's S_CLK to S_CLKOUT9 's length

Part Number: PCI2050B

Hi all :

I am using PCI2050B ,and i have a question about PCI2050B 's S_CLK.

The datasheet said it should connect with S_CLKOUT9 and the trace length should be the same with other S_CLKOUT to the device .

From PCI2050B to Device,there have two connector,so the other S_CLKOUT to the device 's trace length can calculate : (PCI2050B to Connector1) + (connector1 to connector2) + (connector2 to device).

So ,the S_CLK to S_CLKOUT9 's trace length shall be same ?For example,(PCI2050B to Connector1) + (connector1 to connector2) + (connector2 to device)=5000mil,then the S_CLK to S_CLKOUT9 shall route 5000mil?

Because there have two connector ,whether shall i add some length to 5000mil?and how many length shall i add ? What relationship should I follow about the S_CLK to S_CLKOUT9 and other S_CLKOUTs to devices?

Please help me ,thank you very much.

Looking forward to your reply.