Part Number: TUSB8020B
Hello everyone, and Merry Christmas!
I have an MCU to which I have only one USB3.0 interface, so I decided to use a HUB. But I have some concerns and would like to confirm a few things about TUSB8020B.
1- The MCU is the one that must be common point. The other 2 USB sources must go to the MCU, so the MCU is the one that is linked to the upstream port, right?
2- The MCU's USB communicates with both a Module through USB connection but without VBUS on one hand, and an external USB-A connector that comes with a USB_VBUS on the other hand. So I attached the USB_VBUS of the MCU to an external source (5V power supply on the board). In this case, we do not need to use the power switch, do we? So no PWRCTL, no OVERCURxZ, pull-up on FULLPWRMGMT (power switch not supported), and I would put a pull down on GANGED or NC?
3- I saw on an other thread this answer: "TUSB8020B is an active part of the USB system, so RX of the upstream port goes to TX of the host and TX of the upstream port goes to the RX of the host. Likewise, the RX of the downstream port goes to TX of the device and TX of the downstream port goes to RX of the device. It would look like the bottom drawing in the photo that was attached." Here is the link to the thread to see the image they are talking about: https://e2e.ti.com/support/interface/f/138/t/755697?tisearch=e2e-sitesearch&keymatch=TUSB8020B%252525252520power%252525252520switch
But it is not the case from what I see on the Dev board, TX is attached to TX and RX to RX on both upstream and downstream. Are they talking about the internal function of the hub?
Thank you, and happy holidays!