Part Number: TPS25831-Q1
For TPS25831-Q1, when the ambient temperature achieve thermal warning threshold, TPS25831-Q1 will change the advertisement to 1.5A. I am confused that whether 831 can source >1.5A to phone/load or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25831-Q1
For TPS25831-Q1, when the ambient temperature achieve thermal warning threshold, TPS25831-Q1 will change the advertisement to 1.5A. I am confused that whether 831 can source >1.5A to phone/load or not?
Hi Charlie,
The TPS25831-Q1 max loading can up to 5V/3.5A.
It should meet your application requirement