This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25850-Q1: For TPS25850-Q1, can I add a 0.1A load to SENSE pin? Does it have any effect?

Part Number: TPS25850-Q1

For TPS25850-Q1, can I add a 0.1A load to SENSE pin? Does it have any effect?

  • Hi Cora,

    You can refer to page6 about SENSE description.

    It's prohibited to add any load at SENSE pin.

    You can add it at OUT pin which has 200mA capability.

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.