Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: USB-2-MDIO,
I have tried installing, uninstalling, and reinstalling the
MSP430_FET_Drivers
as instructed in the user guide, but when I connect a USB cable, I get no COM port showing up - and no indication that a USB device was connected/disconnected from my computer.
I looked in the install logs and it does appear to be getting an error - even though none is shown in the GUI. The last part of the log is below:
Script stderr:
Executing C:\ti\fetdrivers\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\fetdrivers\emulation\drivers\msp430\USB_CDC"
Script exit code: 256
Script output:
Script stderr:
Program ended with an error exit code
Error running C:\ti\fetdrivers\emulation\drivers\msp430\DPInst\DPinst64.exe /q /se /sa /lm /path "C:\ti\fetdrivers\emulation\drivers\msp430\USB_CDC": Program ended with an error exit code
Creating Uninstaller
Creating uninstaller 25%
Creating uninstaller 50%
Creating uninstaller 75%
Creating uninstaller 100%
Installation completed
Log finished 12/28/2020 at 11:08:04
Mike.