Part Number: TCA9554A
Other Parts Discussed in Thread: TCA9554
hi team,
I want to use 1pcs TCA9554 or TCA9554A to expand GPIO,these GPIO will connect to some signal of Optical module which will be hot insert into our board.
So I want to know does TCA9554 or TCA9554A support hot insert? Or does it support the application scenarios I mentioned above? If not, can you help recommend a more suitable one?
Both input voltage and output voltage are 3.3V, and communication speed is <1kHz.
thanks.