Other Parts Discussed in Thread: TS3USB221
We are designing a device, which has 2 USB C ports. Those USB C ports are in USB 2.0 compatibility mode and are not PD capable.
Our requirements are that the the device can be plugged to a host from any of the 2 USB ports. The second USB port can then be used as downstream for a low power device (such as a mouse).
There is also a MCU on the device that is also connected with USB. The device is also bus powered from the host.
Is there any proposed solution for a usb hub that can do the above?