Other Parts Discussed in Thread: UCC27517, SN74AHCT1G125
Hi,
We have 2 buffers from the same IC connected in parallel. P/N is SN74LVC2G17DBVT.6170.schematic.pdf
Output load is 50 Ohms after 1m cable + polyswitch. (see attached schematic)
Sometimes, the buffer burns.
Then output signal swing is 2V to 5V, instead of 0V to 5V.
* Is it allowed to have 2 buffers in parallel ?
* We source or sink 100mA. Normally 50mA for each buffer. Is this OK ? (according to absolute maximum ratings)
Best regards
Michel