Part Number: TUSB4041I
Hi Team:
Could you please knidly help review the design with TUSB4041I ? Any improvement sugguestions will be appreciated. Thanks in advance.
Best Regards,
Tess Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Hi Team:
Could you please knidly help review the design with TUSB4041I ? Any improvement sugguestions will be appreciated. Thanks in advance.
Best Regards,
Tess Chen
schematic looks good, power switching is not supported?
Hi Tess,
A few more comments on the schematic:
SMBUSz should not be pulled low unless a SMBUS host will be used to configure the hub after power on or the hub will not function.
USB_VBUS is a detection input and needs to be connected to a signal that is high when a host is connected. It should be connected through a resistor divider network so it switches to around 500 mV when on.
The hub is configured as ganged with no power switches, is that correct?
Regards,
JMMN
Hi JMMN,
Thanks for your prompt feedback. The hub is configured as ganged with power switch. Please find the power switch schematic in the attachment.TPS2001C.pdf
Hi Tess,
If separate power switches are enabled for each port, the hub is not ganged (GANGED = 0), and full power management is enabled (FULLPWRMGMTz = 0). So the application can use the internal PU/PD settings for these pin configurations.
Thanks,
JMMN