Part Number: TCA9801
Other Parts Discussed in Thread: TCA9617B, TCA9509
Hey,
actually I have some issues with the I2C bus using ti components. I have connected the TCA9801->B and TCA9617->B Side. I have some undershooting issues which may be resolved by a series resistance. But there is also some kind of square wave on scl + sda when bus is pulled low.... this is alternating so high(up to 0.58V which is > 0.4V) that it causes errors on the i2c, the slaves don't acknoledge. I have read the datasheets + recommendations but I didnt come to a solution.
When connecting both sides to other i2c debugging tool or master/slaves they work good, so there might be some issue with TCA9801->B and TCA9617->B. But considering the datasheets it shall be okay if I understood everything correctly...
Maybe you have some idea ... Thanks for your help!