Part Number: TUSB4041I-Q1
Hello,
Kindly review the attached design using TUSB4041IPAPRQ1
Thanks,
Melbin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I-Q1
Hello,
Kindly review the attached design using TUSB4041IPAPRQ1
Thanks,
Melbin
Hello,
We are working on a project with TUSB4041IPAPRQ1 in it.
Kindly review the attached schematics and let me know the review comments.
we will review and give comment soon
Hi Melbin,
This tiered hub design looks to be part of an embedded application with no exposed standard USB ports, so the port power switching does not need to be used. Is that correct?
Please note that the USB_VBUS input is a detection input and should only be high when an active upstream connection is connected to hub, there can be interoperability issues with connecting it directly to a power rail. Two concerns are having USB_VBUS high while the host is inactive or not powered, and having USB_VBUS held high during reset (GRSTz).
Regards,
JMMN
Hi Melbin,
For USB compliance a hub should always implement overcurrent reporting, FULLPWRMGMTz should be set high to indicate that port power switching is not enabled, and any permanently connected port should be marked as non-removable using EEPROM or SMBUS. If this is an embedded application that will not be required to obtain a USB logo, these are not functionally required.
Please note that USB_VBUS is a detection input and should only be high when an active upstream connection is available. Tying it directly to a power rail may cause interoperability issues.
Regards,
JMMN
Melbin,
I noticed that you have already posted this. In an effort to consolidate posts on E2E, I have merged the threads.
Best,
Danny
Dear JMMN,
The power V_HUB0_3P3 is high only when the Host is active or powered. The MOSFET logic implemented at the top is for that purpose.
What is the issue of a high signal present at USB_VBUS during the reset?
We have not provided external control for the reset pin GRSTZ.
How can I implement the overcurrent reporting?
The devices connected to the down-streams are fixed, but is it necessary to mark them as non-removable using EEPROM or SMBUS?
Hi Melbin,
It appears that the MOSFET logic ensures the proper power up sequencing, does it also ensure that the power is only high when the host is active or powered?
If this is an embedded system that does not require a USB logo, overcurrent reporting is not required. Overcurrent events would typically be reported to the hub OVRCURz inputs from the downstream port power switches for the exposed ports.
For the hub functionality, there is no difference in behavior if a port is marked removable or non-removable, this is only a USB-IF compliance requirement.
Regards,
JMMN
Dear Jimm,
I n this case, can I just pull the pin FULLPWRMGMTZ to high and maintain the remaining section as it is?