Part Number: DP83869HM
Hi I would like to know what the power consumption is for the two voltage supply configuration so VDD1P1 and VDD2P5 when the below interface is used
RGMII to copper 10/100/1000 speeds
Many thanks Andy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83869HM
Hi I would like to know what the power consumption is for the two voltage supply configuration so VDD1P1 and VDD2P5 when the below interface is used
RGMII to copper 10/100/1000 speeds
Many thanks Andy
Hi Andrew,
I've provided the power supply current consumption values for RGMII to Copper mode across speeds below:
| Power Supply Rail | Operational Mode | Typical | Unit |
| I(1V1) | RGMII to Copper (1G) | 131 | mA |
| I(1V1) | RGMII to Copper (100M) | 47 | mA |
| I(1V1) | RGMII to Copper (10M) | 37 | mA |
| I(2V5) | RGMII to Copper (1G) | 86 | mA |
| I(2V5) | RGMII to Copper (100M) | 46 | mA |
| I(2V5) | RGMII to Copper (10M) | 76 | mA |
| I(VDDIO=3.3V) | RGMII to Copper (1G) | 30 | mA |
| I(VDDIO=3.3V) | RGMII to Copper (100M) | 13 | mA |
| I(VDDIO=3.3V) | RGMII to Copper (10M) | 10 | mA |
| I(VDDIO=1.8V) | RGMII to Copper (1G) | 17 | mA |
| I(VDDIO=1.8V) | RGMII to Copper (100M) | 6 | mA |
| I(VDDIO=1.8V) | RGMII to Copper (10M) | 5 | mA |
Regards,
Justin