Part Number: TCA9509
Hi team,
I see VCCA ≤ (VCCB – 1 V) should be true in datasheet, but I found in a customer project, the I2C communication works fine with VCCA=VCCB=3.3V. Could you pls explain the requirement of VCCA ≤ (VCCB – 1 V) from internal circuit point of view? I would like to find the reason that if this part can support VCCA=VCCB in some situations.
Their schematics is like below, but slave voltage level is 3.3V. (change 1.65V to 3.3V)
Thanks.