Part Number: TPS65987D
Hi,
I am attempting to get my power board working in all the various different modes and am having an issue when I plug in a USB-C load or sink. I have a flash drive type stick that I plug in and the port needs to supply 5V to the device.
My controller is configured as a DRP and is toggling the CC lines when nothing is connected. When I plug the device in it changes the CC line toggling pattern to be slower but then has some unknown error. I can see that the TPS chip never connects the power path but have no idea why.
I have attached several screen captures of the GUI tool output as well as a PD analyzer. The PD analyzer shows zero volts and amps on the Vbus lines. Lastly the PD state log is attached but its unclear if this log is ascending or descending time.