This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB564: how to save TUSB564 power consumption if PC is in sleep mode?

Part Number: TUSB564
Other Parts Discussed in Thread: TPS65987

hi Sir,

my customer application is DP UFP device(no usb3) with battery. when PC is in sleep mode, TUSB564 still works with full power. there is AUX snoop feature for power saving. due to the note in datasheet below, they don't know if they can enable this feature or not.

When TUSB564’s AUX snoop feature is enabled, the syncs defined by the DisplayPort
standard must be received in order for AUX snoop feature to function properly. AUX writes
to panel’s DPCD address 0x00600 and 0x00101 should result in SET_POWER_STATE
and LANE_COUNT_SET fields at TUSB564’s offset 0x12 to get set to the appropriate
value. If these fields do not get set correctly, then incoming AUX may not be compliant. If
this is the case, then it is best to disable AUX snoop by setting the
AUX_SNOOP_DISABLE field at offset 0x13.

any information to help customer to do the risk assessment if they enable the AUX snoop feature?

any other suggest to help the TUSB564 power saving when external DP source is in sleep mode?

BR,

frank