Part Number: SN65DPHY440SS
Hi, there,
Good day.
I'm a EE from iEi corp.
We're evaluating to add a re-timer/re-driver for CSI-MIPI transmitting on a handheld medical device.
CSI-MIPI source is a CMOS Sensor (OVM7695) resolution is 640*480*30fps.
Data format is RAW, and MIPI clock rate is 48MHz, data rate is 96MHz.
The total transmitting length might up to 20cm.
Please refer to attached structure.
Questions to consult,
1. Will re-driver/re-timer be needed for 20cm length transmitting?
2. Does SN65DPHY440SS support 1 lane MIPI input?
3. Clock rate is 48MHz, data rate is 96MHz, does SN65DPHY440SS support?
4. If the answer to Q2/Q3 is negative, are there any solutions could be suggested?
Thanks,
Russ