Part Number: TPS65987D
Hi,
I am using TPS65987DDHRSHR for PD in USB type C in SINK only mode, i want to negotiate power at 15, 20V with 5A and i am confused whether i need to put the push buttons at 20V_PB_SINK and 15V_PB_SINK which are in EVM, and do i need any flash memory?
NOTE: C type connector is used only for power and no data lines are connected