Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: TPD1E05U06-Q1, TPD1E0B04, TPD1E01B04
Hello Community,
I have three options to protect FPDlink bus against ESD
PART CL Vwrv Vbreak Vclamp Type
- TPD1E05U06-Q1 0.5pF 5.5V 8.7V 14V Diode
- TPD1E0B04 0.18pF 3.6V 6.7V 10.1V Diode
- CGA0603MLC-05E 0.2pF 5.0V - 30V ChipGuard
with regard to CL, I expect to have a low value with any option so no impact on signal integrity from these devices, nevertheless I am not sure with the clamp voltages.
These are the only values I can get from the datasheet.
Any recommendation for any specific component mentioned above or just go for the one with best price?
Regards
Francisco Gomez