Other Parts Discussed in Thread: TLK1501, TLK3131
I have a customer asking the following:
-----------------------------------------------------------
We have a design which had a TLK1501 put on it as a backup path to an FPGA. We would like to pass Ethernet traffic through it, but after reading the datasheet closer, it is not obvious to us that the part is capable of doing that. Is there a way to do so?
Two problems that jump out include:
1. Every mention in the datasheet of K23.7 (also known as /R/) refers to always transmitting or receiving TWO K23.7 bytes. In Ethernet, the second /R/ is only used on odd length packets.
2. There are no references to how to transmit a K29.7 (/T/) or K27.7 (/S/)
Is there is any possible way to use this for Ethernet?
------------------------------------------------------------------------