Part Number: DP83822I
Other Parts Discussed in Thread: AM3352
Hi,
I use AM3352 along with DP83822I on my custom board.
The ETH uses an RMII in master mode.
The ETH is working correctly, but I have to set registers via MDIO during OS boot.
I use the following sequence to configure DP83822I:
// write 0x4300 to 0x462 extended register mii write 1 0d 1f mii write 1 0e 462 mii write 1 0d 401f mii write 1 0e 4300 // write 0x61 to 0x17 register mii write 1 17 61 // PHY reset mii write 1 1f 4000
Questions:
1) Do I configure this registers correctly to switch DP83822I into RMII master mode?
2) Can I configure the DP83822I to work in this configuration using bootstrap resistors and not the MDIO interface?
Regards
Adam