Part Number: TMDS351
Other Parts Discussed in Thread: TMDS361B
Hi
the datasheet mentioned 12bit color depth.
Is it for each color? Hence 36bit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
It also depends on the chroma subsampling. If the subsampling is 4:4:4, then it is 12x3 = 36 bits per pixel.
Thanks
David
Hi,
Please see the Switching Characteristics spec in the TMDS351 datasheet. Once the TMDS351 switches from one port to the other port, the source supplies 5V to the sink. The sink will only drive the HPD high once its EDID is ready. The source will sample the HPD high and then read the sink EDID, and outputs the video. So the time will vary from source to source, and from sink to sink.
Thanks
David
Hi,
The audio is not being supported by the DVI.
Also the DVI doesn’t support HDCP encryption by default, so you may not be able to play back full HD Blu-rays and other HD content.
Thanks
David