This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002A: Re-driver Impedance during Power On and Receive Detect Phase

Part Number: TUSB1002A


Hi, 

I wanted to use this re-driver with intel platform.

From the platform requirement on the USB3.2 re-driver, it stated :


It is recommended that OEMs use active mux/retimer/redriver parts from 3rd party vendors which meet below requirements to avoid Electrical Over Stress (EOS) on USB 3.2 receiver lines: During power on and receive detect phase, recommended transmitter common mode voltage (Vcm) and impedance values: 

(i) If (Vcm <= 1.2V), Repeater Impedance >= 1K ohm ELSE; 

(ii) (Vcm+Rx.detect pulse amplitude <= 2.2V) AND (Repeater Impedance >= 4.5K ohm).

 

Is the TUSB1002a comply with these requirements?

 

Thank you.

 

-Desmond