Part Number: DS90UB936-Q1
Our system is FPGA<==CSI==DS90UB936<==FPD-link III ==DS90UB935<==CSI==Image Sensor
935 is configured through 936 remote I2C. Format is raw10 2lane, 720Mbps/lane. Can you help provide a configuration of 936 and 935? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB936-Q1
Our system is FPGA<==CSI==DS90UB936<==FPD-link III ==DS90UB935<==CSI==Image Sensor
935 is configured through 936 remote I2C. Format is raw10 2lane, 720Mbps/lane. Can you help provide a configuration of 936 and 935? Thanks!
Hello Andrew,
which device is using 2 lanes? SER or DES?
Which lane speed is 720Mnps? SER or DES?
All required configurations should be done via hardware. If these are correct as per d/s, then the link should be plug and play!!