Part Number: DP83867IR
Hi all,
i am currently in the verification process of a custom hardware design including the DP83867IRRGZ. During the ethernet 1000BaseT compliance tests according to IEE 802 i noticed, that we do not pass some of the mask tests and also the transmitter distortion test. We use a measurement setup from Rohde and Schwarz.
Find some examples of failing tests below:
This is an example of a mask test. The point where the mask is violated is slightly covered by the window in the top left:
And the result of the transmitter distortion test as reported by the compliance tool:
During the transmitter distortion test, the eye looks like follows which is not too bad i think. Are there any reference Screenshots available how the eye should look like?
I followed the process suggested in SNLA239A. Also i am aware of the troubleshouting guide SNLA246 and i checked everything included there.
At first i thought that the hardware on the MDI side of the PHY (e.g. ESD-protection, magnetics) might cause a problem. So i removed everything and added a 100 Ohm differential termination on the pads where usually the magnetics are. So the test setup contains only of the PHY, about 35 mm PCB trace and 4 100 Ohm termination resistors. The measurement results look absolutely the same which makes me wonder if there are any known problems with the PHY?
With best regards
Michael