Part Number: TCA9534
TCA9534 Vcc =3.3V, interrupt pin is open-drain , this pin can be pulled up to 1.8V ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9534
TCA9534 Vcc =3.3V, interrupt pin is open-drain , this pin can be pulled up to 1.8V ?
Hi Cooper,
Yes, since the INT is open-drain it can support any pull up Vcc so long as it is within the recommended operating conditions and tied from INT to Vcc using a resistor (do not tie INT directly to Vcc without some kind of resistance).
-Bobby
Dear Bobby:
Sorry that I double confirm with you, my mean is that Vcc pin actually connected to 3.3V power supply, now customer wants to connect INT to 1.8V with a resisitor, now INT pull high power is different from Vcc. is it ok ?