Part Number: SN65DSI84
Hi team,
Good day.
The datasheet Table 7-8. CSR Bit Field Definitions – LVDS Registers 0x18 address bits 2 and 3 states the following:
Bit3: 1 – Force 24bpp; LVDS channel A lane 4 (B_Y3P/N) is enabled
Bit2: 0 – Force 18bpp; LVDS channel B lane 4 (A_Y3P/N) is disabled (default)
Can you please clarify if this is a typographical error and should be as follows?
Bit3: 1 – Force 24bpp; LVDS channel A lane 4 (A_Y3P/N) is enabled
Bit2: 0 – Force 18bpp; LVDS channel B lane 4 (B_Y3P/N) is disabled (default)
Regards,
Carlo