Part Number: TPS65987D
Hello ,
I wanted to ask about power path and dead battery mode.
I have made a FW for TPS65987D with the Application Customization Tool 6.1.1.
This firmware was supposed to negotiate 5V 3A and keep the power paths open , so that it doesn't pass to PP_HV. I have these paths as disabled , but i still want it to negotiate the 5V 3A contract and enter Alternate mode for Displayport, but it doesn't communicate at all. No traces seen with PD analyzer. Any help ? Why doesn't it negotiate? Is it because the paths are disabled? And how about Entering DisplayPort alternate mode ? Can i enter it if i don't have a power contract?
Added the project: TPS_FW.pjt
Best regards,
Eriks