Part Number: TCA4307
Hello,
I am designing a host with an I2C master that is connected to a I2C slave device.
Most of the time, the host is deep sleeping, and I want to make sure the system consumes very low power when deepsleeping.
In deepsleep, the I2C bus SDA/SCL are HiZ.
1) Is it sufficient to put the TCA4307 into shutdown mode ? Or do I need to put the ENABLE pin to Low ?
2) Unfortunately I can not control the enable pin, so I need to connect it to Vcc ?
I can however control the Vcc of the TCA4307 (and I2C device attached to it).
What if I switch-off the slave power when in deep sleep mode ?
Thanks,
Charles