Part Number: TCA9543A
Hi,
Can I reset TCA9543 via SMBUS command ?
Please refer to below snapshot , the command I marked shows reset default state , does it mean we can use this command to reset TCA9543A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jim,
Thanks for reaching out! The TCA9543A can be reset in either of two ways:
These allow the device to be reset in case of a stuck bus situation. The datasheet section you included indicates that the value of the control register will be 0x00 upon startup or after one of these reset cases. This means that triggering a reset closes both channels, and none will be selected.
There is not a way to formally reset the device via a command over SDA/SCL, but you can achieve the same state by turning off both channels to achieve 0x00 in the control register.
When using the reset functionality, many times, this is done due to a stuck bus that is preventing communication, which would render a reset command via the bus effectively powerless. The RESET pin and the POR both would override the status of the bus.
Best,
Danny