Part Number: TCAN1046V-Q1
Hi,
I am using TCAN1046V-Q1 (2 port trx) to connect two nodes on the same bus. I am using it in the configuration with CANH1 / CANH2, CANL1 / CANL2 respectively shorted. Is this a configuration that could have communication problems? I ask this because I am observing communication failures if the nodes on the bus are only the two driven by TCAN1046V-Q1, while if you add a third node to the bus everything works correctly, even the communication between the first two nodes. If the third node is connected to the bus while off, the communication between the first two nodes continues to be problematic.
Could you please help me?
BR,
Antonio